Resetting LPC546xx while writing to external static RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Resetting LPC546xx while writing to external static RAM

ソリューションへジャンプ
2,559件の閲覧回数
vijo
Contributor III

Hi there,

ref. LPC546xx datasheet fig.25 External static memory read/write access

Does a low on the reset pin abort an external write cycle - if going low in the WR5 window - with a chance for leaving garbage in the addressed SRAM location?

Or will the reset action be delayed until the writecycle has finished?

Just short - is the action of a low reset asynchronous or synchronous with what the CPU is actually doing.

Best regards

Viggo

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,458件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Viggo,

Yes, a reset event of the EMC module immediately aborts a memory write cycle to a external SRAM.

BR

Xiangjun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,458件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Viggo,

If you clear the EMCSYSCTRL[EMCRD] bit, both the POR RESET event and the Reset Pin/Watchdog Reset events can reset the EMC module.

If you set the EMCSYSCTRL[EMCRD] bit, only the POR RESET event can reset the EMC module, The Reset pin/Watchdog reset events can not reset the EMC module in the condition.

Once the EMC module is reset, all registers and functions of the EMC are initialized to it's Reset states immediately, in other words, the Reset event is asynchronous with the CPU action.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,458件の閲覧回数
vijo
Contributor III

thank you for the information TIC,

will a reset of the EMC module immediately abort a memory write cycle to a external SRAM ?

regards

Viggo

0 件の賞賛
返信
2,459件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Viggo,

Yes, a reset event of the EMC module immediately aborts a memory write cycle to a external SRAM.

BR

Xiangjun Rong

0 件の賞賛
返信