Replacement for LPC2388FBD144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Replacement for LPC2388FBD144

2,954 Views
perdrix
Contributor II

These were readily available until recently but now they are only available with an MOQ of a full tray of 300 and a lead time of a whole year.

Clearly NXP don't want us to use these, and this is causing us quite a problem.

So please what is the recommended replacement (preferably pin and code compatible).

Thanks, David

0 Kudos
Reply
6 Replies

2,671 Views
perdrix
Contributor II

LPC4088 has been recommended to me if that would help.   I think you'd need to re-spin the PCB and do a fair bit of work to the s/w though (not looked at that yet).

D.

0 Kudos
Reply

2,666 Views
no_po
Contributor I

Thank you very much for that hint!

I'll have a look on the LPC4088...

0 Kudos
Reply

2,924 Views
perdrix
Contributor II

Thank you - I'll let the relevant folks  know.  Will code built for the LPC2388 run correctly on the LPC1788?

Thanks, David

0 Kudos
Reply

2,919 Views
converse
Senior Contributor V

No. It is a different machine architecture (Cortex-M3 vs ARM7TDMI). So, you need to recompile, and also rewrite some code - the interrupt structure is different, the startup is different and I don't think that the peripherals are 100% compatible. You can probably re-use your own business logic, but the peripheral drivers are going to need work.

2,933 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi perdrix

The pinout of LPC178x/7x is intended to allow pin function compatibility with the LPC24xx
and LPC23xx.

You can consider LPC1778FBD144 as replacement for your part.

Have a nice day,

Jun Zhang

 

0 Kudos
Reply

2,675 Views
no_po
Contributor I

Hello,
I have the same issu with the LPC2388. We have to update our hardware and therefore we also look for a substitution for the 2388.
I'm not sure if the life time of the 1778 will also come to an end in the near future...
Is there another suggestion which is more future proof?
BR
Norbert

0 Kudos
Reply