Replacement LPC2132/36

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Replacement LPC2132/36

1,600 次查看
muhammad_rezan
Contributor I

The longevity of LPC2132/36 will be end at 2021.

pastedImage_1.png

Is it have other MCU which pin to pin compatible with LPC2132/36?

If no, is it in future NXP planned to produce replacement MCU for LPC2132/36 which pin to pin compatible?

Thanks.

0 项奖励
回复
2 回复数

1,464 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Muhammad,

There is an application note for migrating from LPC2xxx to a LPC17xx devices. You could refer to AN10878 at the following link:

https://www.nxp.com/docs/en/application-note/AN10878.pdf

 

However, the direct pin-to-pin replacements are for LPC2300/2400. In case of the LPC2132/36, which has up to 512KB Flash and up to 32KB RAM; an option could be considering the LPC5410x MCUs, based on Cortex M4 core at 100MHz (with optional secondary Cortex M0+ core), many peripherals, up to 512KB Flash and up to 104KB RAM, available on LQFP64 package:

LPC541XX|NXP 


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,464 次查看
muhammad_rezan
Contributor I

Hi Carlos,

Thank you for your information.

Unfortunately both are not suitable to direct replace LPC2132/36.

Is it NXP planned to do it in future?

0 项奖励
回复