Problem with System Core Clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with System Core Clock

1,654 Views
athmesh_n
Contributor IV

Hi,

 I am using LPC1754FBD80 controller, as per datasheet max clock rate is 100MHz. But after the running the code, SystemCoreClock is showing 120MHz as value. 

Where is the issue? 

Labels (4)
1 Reply

1,548 Views
nxf54947
NXP Employee
NXP Employee

Hi athmesh.n

Could you attach a screenshot of  where you found  that SystemCoreClock is equal to 120 MHz?


Best regards,

Ruben