Problem with System Core Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with System Core Clock

1,747件の閲覧回数
athmesh_n
Contributor IV

Hi,

 I am using LPC1754FBD80 controller, as per datasheet max clock rate is 100MHz. But after the running the code, SystemCoreClock is showing 120MHz as value. 

Where is the issue? 

ラベル(4)
1 返信

1,641件の閲覧回数
nxf54947
NXP Employee
NXP Employee

Hi athmesh.n

Could you attach a screenshot of  where you found  that SystemCoreClock is equal to 120 MHz?


Best regards,

Ruben