OM13092 Relocating Data at Board_SDRAM Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM13092 Relocating Data at Board_SDRAM Problem

2,540 次查看
fatihozen
Contributor IV

Hi,

I have LPCXpresso54608 evaluation board ( OM13092 ). I use Mcuxpresso Ide and sdk examples. I chose one of sdk examples and wanted to relocate all data in external sdram. I added pin_mux.c settings to use sdram and used a function to init sdram in main function ( BOARD_InitSDRAM() ). Then, I built and released project. 

I got a linker script file ( driver_examples_emc_emc_sdram_Release.ld ) at the location

"\MCUXpressoIDE_10.1.1_606\workspace\driver_examples_emc_emc_sdram\Release".

Opened it and arranged little bit and activated it from Project menu. Project>Properties>C/C++ Build>Settings>Tool Settings>MCU Linker>Managed Linker Script. Deactivated Manage linker scripts and selected my own linker script and its path.

I know almost nothing about linker scripts file so I might(definitely did) make a mistake. and then I see datas and others files located in Board_Sdram. But I could not press 'Resume Debug Session' button because it was unvisible. I pressed button 'Terminate All debug Sessions' and I got a new error window I made a mistake somewhere and I am asking where I might make a mistake ?

pastedImage_10.png

pastedImage_7.png

pastedImage_9.pngpastedImage_6.png

What did I do in Release.ld file? Here it is.( just deleted all 'SRAM_0_1_2_3' texts and wrote 'BOARD_SDRAM' instead.)

/*
* GENERATED FILE - DO NOT EDIT
* (c) Code Red Technologies Ltd, 2008-2013
* (c) NXP Semiconductors 2013-2018
* Generated linker script file for LPC54608J512
* Created from linkscript.ldt by FMCreateLinkLibraries
* Using Freemarker v2.3.23
* MCUXpresso IDE v10.1.1 [Build 606] [2018-01-02] on Mar 14, 2018 1:57:33 PM
*/

INCLUDE "mmdriver_examples_emc_emc_sdram_Release_library.ld"
INCLUDE "mmdriver_examples_emc_emc_sdram_Release_memory.ld"

ENTRY(ResetISR)

SECTIONS
{
.text_Flash2 : ALIGN(4)
{
FILL(0xff)
*(.text_Flash2*) /* for compatibility with previous releases */
*(.text_BOARD_FLASH*) /* for compatibility with previous releases */
*(.text.$Flash2*)
*(.text.$BOARD_FLASH*) *(.rodata.$Flash2*)
*(.rodata.$BOARD_FLASH*) } > BOARD_FLASH

/* MAIN TEXT SECTION */
.text : ALIGN(4)
{
FILL(0xff)
__vectors_start__ = ABSOLUTE(.) ;
KEEP(*(.isr_vector))
/* Global Section Table */
. = ALIGN(4) ;
__section_table_start = .;
__data_section_table = .;
LONG(LOADADDR(.data));
LONG( ADDR(.data));
LONG( SIZEOF(.data));
LONG(LOADADDR(.data_RAM2));
LONG( ADDR(.data_RAM2));
LONG( SIZEOF(.data_RAM2));
LONG(LOADADDR(.data_RAM3));
LONG( ADDR(.data_RAM3));
LONG( SIZEOF(.data_RAM3));
LONG(LOADADDR(.data_RAM4));
LONG( ADDR(.data_RAM4));
LONG( SIZEOF(.data_RAM4));
__data_section_table_end = .;
__bss_section_table = .;
LONG( ADDR(.bss));
LONG( SIZEOF(.bss));
LONG( ADDR(.bss_RAM2));
LONG( SIZEOF(.bss_RAM2));
LONG( ADDR(.bss_RAM3));
LONG( SIZEOF(.bss_RAM3));
LONG( ADDR(.bss_RAM4));
LONG( SIZEOF(.bss_RAM4));
__bss_section_table_end = .;
__section_table_end = . ;
/* End of Global Section Table */

*(.after_vectors*)

} >PROGRAM_FLASH

.text : ALIGN(4)
{
*(.text*)
*(.rodata .rodata.* .constdata .constdata.*)
. = ALIGN(4);
} > PROGRAM_FLASH
/*
* for exception handling/unwind - some Newlib functions (in common
* with C++ and STDC++) use this.
*/
.ARM.extab : ALIGN(4)
{
*(.ARM.extab* .gnu.linkonce.armextab.*)
} > PROGRAM_FLASH
__exidx_start = .;

.ARM.exidx : ALIGN(4)
{
*(.ARM.exidx* .gnu.linkonce.armexidx.*)
} > PROGRAM_FLASH
__exidx_end = .;

_etext = .;


/* USB_RAM */
.m_usb_data (NOLOAD) :
{
*(m_usb_global)
} > USB_RAM
/* DATA section for SRAMX */
.data_RAM2 : ALIGN(4)
{
FILL(0xff)
PROVIDE(__start_data_RAM2 = .) ;
*(.ramfunc.$RAM2)
*(.ramfunc.$SRAMX)
*(.data.$RAM2*)
*(.data.$SRAMX*)
. = ALIGN(4) ;
PROVIDE(__end_data_RAM2 = .) ;
} > SRAMX AT>PROGRAM_FLASH

/* DATA section for USB_RAM */
.data_RAM3 : ALIGN(4)
{
FILL(0xff)
PROVIDE(__start_data_RAM3 = .) ;
*(.ramfunc.$RAM3)
*(.ramfunc.$USB_RAM)
*(.data.$RAM3*)
*(.data.$USB_RAM*)
. = ALIGN(4) ;
PROVIDE(__end_data_RAM3 = .) ;
} > USB_RAM AT>PROGRAM_FLASH

/* DATA section for BOARD_SDRAM */
.data_RAM4 : ALIGN(4)
{
FILL(0xff)
PROVIDE(__start_data_RAM4 = .) ;
*(.ramfunc.$RAM4)
*(.ramfunc.$BOARD_SDRAM)
*(.data.$RAM4*)
*(.data.$BOARD_SDRAM*)
. = ALIGN(4) ;
PROVIDE(__end_data_RAM4 = .) ;
} > BOARD_SDRAM AT>PROGRAM_FLASH

/* MAIN DATA SECTION */
.uninit_RESERVED : ALIGN(4)
{
KEEP(*(.bss.$RESERVED*))
. = ALIGN(4) ;
_end_uninit_RESERVED = .;
} > BOARD_SDRAM
/* Main DATA section (BOARD_SDRAM) */
.data : ALIGN(4)
{
FILL(0xff)
_data = . ;
*(vtable)
*(.ramfunc*)
*(.data*)
. = ALIGN(4) ;
_edata = . ;
} > BOARD_SDRAM AT>PROGRAM_FLASH
/* BSS section for SRAMX */
.bss_RAM2 : ALIGN(4)
{
PROVIDE(__start_bss_RAM2 = .) ;
*(.bss.$RAM2*)
*(.bss.$SRAMX*)
. = ALIGN (. != 0 ? 4 : 1) ; /* avoid empty segment */
PROVIDE(__end_bss_RAM2 = .) ;
} > SRAMX
/* BSS section for USB_RAM */
.bss_RAM3 : ALIGN(4)
{
PROVIDE(__start_bss_RAM3 = .) ;
*(.bss.$RAM3*)
*(.bss.$USB_RAM*)
. = ALIGN (. != 0 ? 4 : 1) ; /* avoid empty segment */
PROVIDE(__end_bss_RAM3 = .) ;
} > USB_RAM
/* BSS section for BOARD_SDRAM */
.bss_RAM4 : ALIGN(4)
{
PROVIDE(__start_bss_RAM4 = .) ;
*(.bss.$RAM4*)
*(.bss.$BOARD_SDRAM*)
. = ALIGN (. != 0 ? 4 : 1) ; /* avoid empty segment */
PROVIDE(__end_bss_RAM4 = .) ;
} > BOARD_SDRAM
/* MAIN BSS SECTION */
.bss : ALIGN(4)
{
_bss = .;
*(.bss*)
*(COMMON)
. = ALIGN(4) ;
_ebss = .;
PROVIDE(end = .);
} > BOARD_SDRAM
/* NOINIT section for SRAMX */
.noinit_RAM2 (NOLOAD) : ALIGN(4)
{
*(.noinit.$RAM2*)
*(.noinit.$SRAMX*)
. = ALIGN(4) ;
} > SRAMX
/* NOINIT section for USB_RAM */
.noinit_RAM3 (NOLOAD) : ALIGN(4)
{
*(.noinit.$RAM3*)
*(.noinit.$USB_RAM*)
. = ALIGN(4) ;
} > USB_RAM
/* NOINIT section for BOARD_SDRAM */
.noinit_RAM4 (NOLOAD) : ALIGN(4)
{
*(.noinit.$RAM4*)
*(.noinit.$BOARD_SDRAM*)
. = ALIGN(4) ;
} > BOARD_SDRAM
/* DEFAULT NOINIT SECTION */
.noinit (NOLOAD): ALIGN(4)
{
_noinit = .;
*(.noinit*)
. = ALIGN(4) ;
_end_noinit = .;
} > BOARD_SDRAM

/* Reserve and place Heap within memory map */
_HeapSize = 0x1000;
.heap : ALIGN(4)
{
_pvHeapStart = .;
. += _HeapSize;
. = ALIGN(4);
_pvHeapLimit = .;
} > BOARD_SDRAM

_StackSize = 0x1000;
/* Reserve space in memory for Stack */
.heap2stackfill :
{
. += _StackSize;
} > BOARD_SDRAM
/* Locate actual Stack in memory map */
.stack ORIGIN(BOARD_SDRAM) + LENGTH(BOARD_SDRAM) - _StackSize - 0: ALIGN(4)
{
_vStackBase = .;
. = ALIGN(4);
_vStackTop = . + _StackSize;
} > BOARD_SDRAM

/* ## Create checksum value (used in startup) ## */
PROVIDE(__valid_user_code_checksum = 0 -
(_vStackTop
+ (ResetISR + 1)
+ (NMI_Handler + 1)
+ (HardFault_Handler + 1)
+ (( DEFINED(MemManage_Handler) ? MemManage_Handler : 0 ) + 1) /* MemManage_Handler may not be defined */
+ (( DEFINED(BusFault_Handler) ? BusFault_Handler : 0 ) + 1) /* BusFault_Handler may not be defined */
+ (( DEFINED(UsageFault_Handler) ? UsageFault_Handler : 0 ) + 1) /* UsageFault_Handler may not be defined */
) );

/* Provide basic symbols giving location and size of main text
* block, including initial values of RW data sections. Note that
* these will need extending to give a complete picture with
* complex images (e.g multiple Flash banks).
*/
_image_start = LOADADDR(.text);
_image_end = LOADADDR(.data) + SIZEOF(.data);
_image_size = _image_end - _image_start;
}

标签 (2)
0 项奖励
回复
1 回复

2,269 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi  fatih ozen,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
To provide the fastest possible support, I want to point you to refer to the section 11.7 Modifying the generated linker script/ memory layout in the attachment.
Have a great day,
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 项奖励
回复