OM13071 | PC is not detect the USB debug port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13071 | PC is not detect the USB debug port

ソリューションへジャンプ
2,553件の閲覧回数
shai_b
Senior Contributor II

Hi Team,

My customer has used OM13071 (LPC824 devkit) for two weeks and suddenly the USB connector did not open a port on the computer and he can not able to flash/debug anymore.

He even use a bread new EVK and reinstall the LPC11Uxx_Debug_Probe_VCOM drivers 
But still, the debug probe has not been detected by the PC, Could you please suggest how can we resolve this issue?

Waiting for your kind feedback, Thanks a lot.

Regards,

Shai

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,549件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi shai_b 

Please unzip attached firmware.zip and press on board reset button when connecting board with USB cable. then drag firmware.bin to it. 

Please note, the firename must be firmware.bin. don't change it to other name. don't use capital letter.

ZhangJennie_0-1640838286995.png

Power off and power on again. Make sure you have driver installed.

If the board is not broken, it should be recognized by PC.

You could try two more computer to verify this is a board issue or a PC issue. 

 

Hope this helps,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,550件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi shai_b 

Please unzip attached firmware.zip and press on board reset button when connecting board with USB cable. then drag firmware.bin to it. 

Please note, the firename must be firmware.bin. don't change it to other name. don't use capital letter.

ZhangJennie_0-1640838286995.png

Power off and power on again. Make sure you have driver installed.

If the board is not broken, it should be recognized by PC.

You could try two more computer to verify this is a board issue or a PC issue. 

 

Hope this helps,

Jun Zhang

0 件の賞賛
返信
2,524件の閲覧回数
shai_b
Senior Contributor II

@ZhangJennie ,Thank you.

KR,

Shai

0 件の賞賛
返信