NFC in phones

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NFC in phones

跳至解决方案
1,910 次查看
ujwal_kumar_N_L
Contributor III

Hi community 

I'm working on NFC  RC663 ,i have tried reading NFC tags and cards .Im unable to use phone as a card emulator. The NFC id  keeps on changing as the NFC in phones is used for contactless paying .Is there anyway in which i can use some mobile application and make sure the phone send the same id all the time?
Application is that phone acts as a method of accessing the door system .So i need the ID to be constant .

Thank you and regards 
UJWAL

0 项奖励
回复
1 解答
1,897 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. As this is a behavior from the phones, and not related to our CLRC663, I would recommend you contact the phone manufacturer to see if something can be done at their side.

 

I apologize for the inconveniences.

 

Regards,

Ricardo

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,898 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. As this is a behavior from the phones, and not related to our CLRC663, I would recommend you contact the phone manufacturer to see if something can be done at their side.

 

I apologize for the inconveniences.

 

Regards,

Ricardo

0 项奖励
回复