NFC in phones

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,908件の閲覧回数
ujwal_kumar_N_L
Contributor III

Hi community 

I'm working on NFC  RC663 ,i have tried reading NFC tags and cards .Im unable to use phone as a card emulator. The NFC id  keeps on changing as the NFC in phones is used for contactless paying .Is there anyway in which i can use some mobile application and make sure the phone send the same id all the time?
Application is that phone acts as a method of accessing the door system .So i need the ID to be constant .

Thank you and regards 
UJWAL

0 件の賞賛
返信
1 解決策
1,895件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. As this is a behavior from the phones, and not related to our CLRC663, I would recommend you contact the phone manufacturer to see if something can be done at their side.

 

I apologize for the inconveniences.

 

Regards,

Ricardo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,896件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. As this is a behavior from the phones, and not related to our CLRC663, I would recommend you contact the phone manufacturer to see if something can be done at their side.

 

I apologize for the inconveniences.

 

Regards,

Ricardo

0 件の賞賛
返信