More than three DACs.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

More than three DACs.

1,514件の閲覧回数
simoneacciarito
Contributor I

Hi everybody. I need to use an MCU with more than three DACs. Can you tell me if there are MCUs in the lpc family with this requirement? Thanks in advance.

0 件の賞賛
返信
2 返答(返信)

1,428件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately, there is not a LPC device with more than 3 DAC's, you can check the LPC product selector guide in the following link:

https://www.nxp.com/docs/en/product-selector-guide/LPCMICROLNCD.pdf 

I have the same recommendation than Mark in the thread: More than three DAC. 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,428件の閲覧回数
ianbenton
Senior Contributor I

DO you need a ridiculously fast response? If not, use the PWM outputs followed by a RC filter (or even an RCRC filter if you need really low ripple)

0 件の賞賛
返信