More than three DACs.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

More than three DACs.

1,494 Views
simoneacciarito
Contributor I

Hi everybody. I need to use an MCU with more than three DACs. Can you tell me if there are MCUs in the lpc family with this requirement? Thanks in advance.

0 Kudos
Reply
2 Replies

1,408 Views
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately, there is not a LPC device with more than 3 DAC's, you can check the LPC product selector guide in the following link:

https://www.nxp.com/docs/en/product-selector-guide/LPCMICROLNCD.pdf 

I have the same recommendation than Mark in the thread: More than three DAC. 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,408 Views
ianbenton
Senior Contributor I

DO you need a ridiculously fast response? If not, use the PWM outputs followed by a RC filter (or even an RCRC filter if you need really low ripple)

0 Kudos
Reply