Missing SRAM layout of LPC546xx 136KB RAM version in doc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Missing SRAM layout of LPC546xx 136KB RAM version in doc

跳至解决方案
1,446 次查看
zouyao
Contributor I

LPC546XX has 136KB RAM and 256KB flash version, but I cannot find the 136KB SRAM memory map in the reference manual, which all describe RAM as 200KB.

pastedImage_1.png

My question is which is the SRAM layout for 136KB RAM version of LPC546xx (e.g. LPC54605J256ET180)?

0 项奖励
回复
1 解答
1,300 次查看
soledad
NXP Employee
NXP Employee

Hi,

SRAM banks starts from 0x20000000 with size 0x18000(96K)

SRAMX starts from 0x4000000 with size 0x8000(32K)

USB RAM starts from 0x40100000 with size 0x2000 (8K)

 

Sum - 136KB

 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,301 次查看
soledad
NXP Employee
NXP Employee

Hi,

SRAM banks starts from 0x20000000 with size 0x18000(96K)

SRAMX starts from 0x4000000 with size 0x8000(32K)

USB RAM starts from 0x40100000 with size 0x2000 (8K)

 

Sum - 136KB

 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复