Missing SRAM layout of LPC546xx 136KB RAM version in doc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing SRAM layout of LPC546xx 136KB RAM version in doc

ソリューションへジャンプ
2,052件の閲覧回数
zouyao
Contributor I

LPC546XX has 136KB RAM and 256KB flash version, but I cannot find the 136KB SRAM memory map in the reference manual, which all describe RAM as 200KB.

pastedImage_1.png

My question is which is the SRAM layout for 136KB RAM version of LPC546xx (e.g. LPC54605J256ET180)?

ラベル(5)
0 件の賞賛
返信
1 解決策
1,906件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

SRAM banks starts from 0x20000000 with size 0x18000(96K)

SRAMX starts from 0x4000000 with size 0x8000(32K)

USB RAM starts from 0x40100000 with size 0x2000 (8K)

 

Sum - 136KB

 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,907件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

SRAM banks starts from 0x20000000 with size 0x18000(96K)

SRAMX starts from 0x4000000 with size 0x8000(32K)

USB RAM starts from 0x40100000 with size 0x2000 (8K)

 

Sum - 136KB

 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信