MDIO Support on FLEXCOMMs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MDIO Support on FLEXCOMMs

Jump to solution
2,315 Views
Bill6
Contributor II

Greetings,

I'm using an NXP LPC55S28JBD100 to communicate with I2C and MDIO devices. In the MCUXpresso IDE's PINS tool, I see pins in the FLEXCOMM3 display listed as MDIO and MDC. Can FLEXCOMM3 operate as an MDIO master? Or, can I use MDIO on any FLEXCOMM interface?

Sincerely,

Bill Long

ITI Engineering

408-569-3940

0 Kudos
Reply
1 Solution
2,309 Views
Bill6
Contributor II
Hi EdwinHz,

Thank you for the prompt reply. I'm using SDK v2.15.100. I didn't think MDIO was supported but I saw it in the display, so I thought I'd check.

Bill Long

View solution in original post

0 Kudos
Reply
2 Replies
2,311 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Bill6,

What SDK version are you using? I don't see any pin label to be MDIO on the LPC55S28JBD100, because this LPC does not support this feature. Perhaps it's an error on a previous SDK version.

BR,
Edwin.

0 Kudos
Reply
2,310 Views
Bill6
Contributor II
Hi EdwinHz,

Thank you for the prompt reply. I'm using SDK v2.15.100. I didn't think MDIO was supported but I saw it in the display, so I thought I'd check.

Bill Long
0 Kudos
Reply