Libraries/Solutions for TFT Display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Libraries/Solutions for TFT Display

1,949 Views
lucasfontan
Contributor I

HI! Has anyone used a TFT display with ILI9341 integrated circuit using LPCOpen? If anyone has a clue or some help it would be very useful for me.

 

Thanks you!

Tags (1)
0 Kudos
Reply
1 Reply

1,555 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Lucas,

You can use the emwin 5.30 Pre-Compiled Libraries for NXP ARM MCUs, they come with support for the ILI9341 display using the GUIDRV_FlexColor driver, you can find more information and download the library on these links:

http://cache.nxp.com/files/microcontrollers/doc/support_info/UM03001_emWin5_8.pdf

emWin Graphics Library|NXP

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 Kudos
Reply