LS1046A not working now

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A not working now

跳至解决方案
1,659 次查看
Sarthak
Contributor I

Hii,

I am facing an issue with NXP LS1046A RDB. It was working well but suddenly its not connecting to the host. When I try to connect it to a linux host using minicom, it is not getting connected to ttyACM0. It throws "No such file or directory". It is connecting in bootloader mode and the led D8 is blinking .

After performing the usual process when I tap reset button, instead of connecting to tty serial port it is getting detected or connecting as a bootloader.

 

Minicom serial port setup:

| A - Serial Device : /dev/ttyACM0 |
| B - Lockfile Location : /var/lock |
| C - Callin Program : |
| D - Callout Program : |
| E - Bps/Par/Bits : 115200 8N1 |
| F - Hardware Flow Control : Yes |
| G - Software Flow Control : No

 

Error:

minicom: cannot open /dev/ttyACM0: No such file or directory.

Please help me to solve this issue.

Regards

0 项奖励
回复
1 解答
1,635 次查看
frank_m
Senior Contributor III

> Please help me to solve this issue.

The first step is probably to find the proper sub-forum.
This one here deals with MCUs orders of magnitude smaller than your LS1046.
I suspect poster here are not really able to help you ...

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,636 次查看
frank_m
Senior Contributor III

> Please help me to solve this issue.

The first step is probably to find the proper sub-forum.
This one here deals with MCUs orders of magnitude smaller than your LS1046.
I suspect poster here are not really able to help you ...

0 项奖励
回复