LS1046A not working now

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A not working now

Jump to solution
1,736 Views
Sarthak
Contributor I

Hii,

I am facing an issue with NXP LS1046A RDB. It was working well but suddenly its not connecting to the host. When I try to connect it to a linux host using minicom, it is not getting connected to ttyACM0. It throws "No such file or directory". It is connecting in bootloader mode and the led D8 is blinking .

After performing the usual process when I tap reset button, instead of connecting to tty serial port it is getting detected or connecting as a bootloader.

 

Minicom serial port setup:

| A - Serial Device : /dev/ttyACM0 |
| B - Lockfile Location : /var/lock |
| C - Callin Program : |
| D - Callout Program : |
| E - Bps/Par/Bits : 115200 8N1 |
| F - Hardware Flow Control : Yes |
| G - Software Flow Control : No

 

Error:

minicom: cannot open /dev/ttyACM0: No such file or directory.

Please help me to solve this issue.

Regards

0 Kudos
Reply
1 Solution
1,712 Views
frank_m
Senior Contributor III

> Please help me to solve this issue.

The first step is probably to find the proper sub-forum.
This one here deals with MCUs orders of magnitude smaller than your LS1046.
I suspect poster here are not really able to help you ...

View solution in original post

0 Kudos
Reply
1 Reply
1,712 Views
frank_m
Senior Contributor III

> Please help me to solve this issue.

The first step is probably to find the proper sub-forum.
This one here deals with MCUs orders of magnitude smaller than your LS1046.
I suspect poster here are not really able to help you ...

0 Kudos
Reply