LPC84x data retention

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC84x data retention

Jump to solution
3,848 Views
jun1
Contributor V

Hello.

We are considering equipment with a product life of at least 15 years.

The CPU to be used is considered with LPC84x.

It is the data retention period of flash ROM,

The Kinetis series has a minimum of 20 years typ 100 years.

LPC84x is Min 10 years Typ 20 years.

So the question is

1. Test method complies with JEDEC NVM qualification.
     What are the conditions?

2. If temperature conditions are relaxed, will there be a minimum of 20 years?

Thank you.

jun

Labels (1)
Tags (1)
1 Solution
3,658 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello, 

The information I already mentioned is the only one we have available.

Sorry for any inconveniences this may cause you.

Regards,

Sebastian

View solution in original post

6 Replies
3,658 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Jun,

 

1.- For the JEDEC NVM qualification of the LPC-84x, they were subjected while testing to temperatures ranging from -40°C to 150°C.

2.- As you say, typically, you can expect a data retention time of 20 years in regular temperature conditions.

Please look at the image below, and if you want more details, you can refer to the LPC-84x Product Data Sheet: https://www.nxp.com/docs/en/data-sheet/LPC84x.pdf

pastedImage_1.png

Regards,

Sebastian

0 Kudos
Reply
3,658 Views
jun1
Contributor V

Thank you for your reply. I was relieved for the time being.

For further discussion, I would like to receive data for the following reasons. Where can I get it? If you need a procedure, please let us know.

We would like to derive standard usage conditions from the results of environmental stress acceleration tests and predict the effective product life.
I would like to receive data or reports that allow us to understand the environmental conditions that would normally be expected to be 20 years.

Thank you.

jun
(I live in Japan. English is not good)

0 Kudos
Reply
3,658 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Jun,

 

You can find more information about JEDEC's NVM qualification on their website. You will need to register to access the document, but it's free.

 

Regards,

Sebastian

0 Kudos
Reply
3,658 Views
jun1
Contributor V

thank you for your answer.


I saw the site, but it is related
"SOLID STATE DRIVE (SSD) REQUIREMENTS AND ENDURANCE TEST METHOD JESD 218 B. 01 Jun 2016"
I think that, but this was paid.

What should I tell you, if the ambient temperature is 55 ° C, how long will the data retention time be?

Thank you.

jun

0 Kudos
Reply
3,659 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello, 

The information I already mentioned is the only one we have available.

Sorry for any inconveniences this may cause you.

Regards,

Sebastian

3,658 Views
jun1
Contributor V

Thank you very much.
Let's check it by another route.
Have a good day.

0 Kudos
Reply