LPC84x data retention

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC84x data retention

跳至解决方案
3,891 次查看
jun1
Contributor V

Hello.

We are considering equipment with a product life of at least 15 years.

The CPU to be used is considered with LPC84x.

It is the data retention period of flash ROM,

The Kinetis series has a minimum of 20 years typ 100 years.

LPC84x is Min 10 years Typ 20 years.

So the question is

1. Test method complies with JEDEC NVM qualification.
     What are the conditions?

2. If temperature conditions are relaxed, will there be a minimum of 20 years?

Thank you.

jun

标签 (1)
标记 (1)
1 解答
3,701 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello, 

The information I already mentioned is the only one we have available.

Sorry for any inconveniences this may cause you.

Regards,

Sebastian

在原帖中查看解决方案

6 回复数
3,701 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Jun,

 

1.- For the JEDEC NVM qualification of the LPC-84x, they were subjected while testing to temperatures ranging from -40°C to 150°C.

2.- As you say, typically, you can expect a data retention time of 20 years in regular temperature conditions.

Please look at the image below, and if you want more details, you can refer to the LPC-84x Product Data Sheet: https://www.nxp.com/docs/en/data-sheet/LPC84x.pdf

pastedImage_1.png

Regards,

Sebastian

0 项奖励
回复
3,701 次查看
jun1
Contributor V

Thank you for your reply. I was relieved for the time being.

For further discussion, I would like to receive data for the following reasons. Where can I get it? If you need a procedure, please let us know.

We would like to derive standard usage conditions from the results of environmental stress acceleration tests and predict the effective product life.
I would like to receive data or reports that allow us to understand the environmental conditions that would normally be expected to be 20 years.

Thank you.

jun
(I live in Japan. English is not good)

0 项奖励
回复
3,701 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Jun,

 

You can find more information about JEDEC's NVM qualification on their website. You will need to register to access the document, but it's free.

 

Regards,

Sebastian

0 项奖励
回复
3,701 次查看
jun1
Contributor V

thank you for your answer.


I saw the site, but it is related
"SOLID STATE DRIVE (SSD) REQUIREMENTS AND ENDURANCE TEST METHOD JESD 218 B. 01 Jun 2016"
I think that, but this was paid.

What should I tell you, if the ambient temperature is 55 ° C, how long will the data retention time be?

Thank you.

jun

0 项奖励
回复
3,702 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello, 

The information I already mentioned is the only one we have available.

Sorry for any inconveniences this may cause you.

Regards,

Sebastian

3,701 次查看
jun1
Contributor V

Thank you very much.
Let's check it by another route.
Have a good day.

0 项奖励
回复