LPC84x FlashROM Data retention

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC84x FlashROM Data retention

1,898件の閲覧回数
jun1
Contributor V

HI.

1. Is the flash ROM of the LPC84x NOR type?


2. Does this data retention period mean the life is calculated from the number of read errors that occur as a result of accelerated testing with the temperature turned on with the power on?


3. I think that the probability that the error of the flash ROM occurs in the power ON state changes with the temperature condition, for example, when the standard of Tamb = -40 ° C to +105 ° C is relaxed from -20 ° C to +70 ° C etc., the period is extended Is it?
I would be happy if you could tell me the formula.

# I do not think that English is not good.

Thank you.

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,784件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

What do you mean with ROM type NOR, the internal structure? if this is the case this information can not be shared, this is internal information

On the following link, you can see some information about how the data retention is calculated, this is a reference

https://www.nxp.com/docs/en/engineering-bulletin/EB618.pdf

And yes with more temperature range there are more probabilities of failures, but there is not a formula that can be shared 

Regards

1,784件の閲覧回数
jun1
Contributor V

Hi.

I was able to understand the data retention characteristics.

I asked because the LPC series was MIN 10 years.

I understand this matter.

Thank you very much.

0 件の賞賛
返信