LPC812 can not work at 1.8V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC812 can not work at 1.8V

2,861 Views
wwz
Contributor I

hello everyone,

According to the user manual, lpc812 can work at 1.8v-3.6v, but the test results of my side will not work when the voltage is lower than 2.6v, and the BOD function is also disabled. Do I need any special Settings if I want to use 1.8v?

thanks

0 Kudos
Reply
4 Replies

2,842 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you give us more information for example, how do you  know that the LPC812 does not work when the VDD is 2.6V?

Pls use the LED blinky example in SDK and impress 2.6V to the VDD, does the LED still toggle?

If the BOD is disabled, I do not think there is special configuration if you use low voltage VDD.

In 2.6V, if you press Reset, can the board work?

BR

XiangJun Rong

0 Kudos
Reply

2,830 Views
wwz
Contributor I

Hi,

Thanks for the quick response, i have found the problem, it is caused by an external reset chip.but i have another quesiton: for the BOD reset level 0, LPC812 has no description of reset level 0 ,but LPC824 has the description of reset levle 0,Is it the same as LPC824?

thanks & best regards!

Tags (1)
0 Kudos
Reply

2,800 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that there is not reset level 0 for both LPC82x and LPC81x, there are Reset level 1,2,3, which corresponds to different Reset threshold voltage.

For LPC81x:

xiangjun_rong_0-1686881560166.png

 

The corresponding threshold voltage for LPC81x is defined in data sheet of LPC81x:

xiangjun_rong_1-1686881701544.png

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

2,781 Views
wwz
Contributor I

Hi,

OK,

thanks

0 Kudos
Reply