LPC812 can not work at 1.8V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC812 can not work at 1.8V

2,850件の閲覧回数
wwz
Contributor I

hello everyone,

According to the user manual, lpc812 can work at 1.8v-3.6v, but the test results of my side will not work when the voltage is lower than 2.6v, and the BOD function is also disabled. Do I need any special Settings if I want to use 1.8v?

thanks

0 件の賞賛
返信
4 返答(返信)

2,831件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Can you give us more information for example, how do you  know that the LPC812 does not work when the VDD is 2.6V?

Pls use the LED blinky example in SDK and impress 2.6V to the VDD, does the LED still toggle?

If the BOD is disabled, I do not think there is special configuration if you use low voltage VDD.

In 2.6V, if you press Reset, can the board work?

BR

XiangJun Rong

0 件の賞賛
返信

2,819件の閲覧回数
wwz
Contributor I

Hi,

Thanks for the quick response, i have found the problem, it is caused by an external reset chip.but i have another quesiton: for the BOD reset level 0, LPC812 has no description of reset level 0 ,but LPC824 has the description of reset levle 0,Is it the same as LPC824?

thanks & best regards!

タグ(1)
0 件の賞賛
返信

2,789件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that there is not reset level 0 for both LPC82x and LPC81x, there are Reset level 1,2,3, which corresponds to different Reset threshold voltage.

For LPC81x:

xiangjun_rong_0-1686881560166.png

 

The corresponding threshold voltage for LPC81x is defined in data sheet of LPC81x:

xiangjun_rong_1-1686881701544.png

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信

2,770件の閲覧回数
wwz
Contributor I

Hi,

OK,

thanks

0 件の賞賛
返信