LPC804M101JDH20 Max operating Frequency?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC804M101JDH20 Max operating Frequency?

Jump to solution
1,954 Views
wen-lianglin
Contributor I

I found out that there is a part in the LPC80X family that can run up to 180MHz.
Is this true or just a typo?
Other families have similar special products. LPC832M101FDH20.

wenlianglin_0-1692411832404.pngwenlianglin_0-1692411832404.png

 

Labels (1)
0 Kudos
Reply
1 Solution
1,903 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @wen-lianglin 

This was a typo and it's fixed.

Please check again.

Thanks for bringing the problem to our attention.

Jun Zhang

View solution in original post

0 Kudos
Reply
2 Replies
1,904 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @wen-lianglin 

This was a typo and it's fixed.

Please check again.

Thanks for bringing the problem to our attention.

Jun Zhang

0 Kudos
Reply
1,925 Views
frank_m
Senior Contributor III

I suspect this is just a typo.
Especially considering the very similiar devices listed below this entry, which all specify 15MHz. 

AFAIK, ARM's licence conditions don't allow for freestanding M0/M0+ with clock rates beyond 50MHz.

0 Kudos
Reply