LPC804M101JDH20 Max operating Frequency?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC804M101JDH20 Max operating Frequency?

跳至解决方案
2,100 次查看
wen-lianglin
Contributor I

I found out that there is a part in the LPC80X family that can run up to 180MHz.
Is this true or just a typo?
Other families have similar special products. LPC832M101FDH20.

wenlianglin_0-1692411832404.png

 

标签 (1)
0 项奖励
回复
1 解答
2,049 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @wen-lianglin 

This was a typo and it's fixed.

Please check again.

Thanks for bringing the problem to our attention.

Jun Zhang

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,049 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @wen-lianglin 

This was a typo and it's fixed.

Please check again.

Thanks for bringing the problem to our attention.

Jun Zhang

0 项奖励
回复
2,071 次查看
frank_m
Senior Contributor III

I suspect this is just a typo.
Especially considering the very similiar devices listed below this entry, which all specify 15MHz. 

AFAIK, ARM's licence conditions don't allow for freestanding M0/M0+ with clock rates beyond 50MHz.

0 项奖励
回复