LPC804M101JDH20 Max operating Frequency?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC804M101JDH20 Max operating Frequency?

ソリューションへジャンプ
2,007件の閲覧回数
wen-lianglin
Contributor I

I found out that there is a part in the LPC80X family that can run up to 180MHz.
Is this true or just a typo?
Other families have similar special products. LPC832M101FDH20.

wenlianglin_0-1692411832404.png

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,956件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @wen-lianglin 

This was a typo and it's fixed.

Please check again.

Thanks for bringing the problem to our attention.

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,957件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI @wen-lianglin 

This was a typo and it's fixed.

Please check again.

Thanks for bringing the problem to our attention.

Jun Zhang

0 件の賞賛
返信
1,978件の閲覧回数
frank_m
Senior Contributor III

I suspect this is just a typo.
Especially considering the very similiar devices listed below this entry, which all specify 15MHz. 

AFAIK, ARM's licence conditions don't allow for freestanding M0/M0+ with clock rates beyond 50MHz.

0 件の賞賛
返信