LPC804 - MCUXpresso based Secondary Boot Loader (SBL)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC804 - MCUXpresso based Secondary Boot Loader (SBL)

跳至解决方案
3,231 次查看
biju_nair
Contributor III

Hi,

I am looking at an MCUXpresso based project for LPC804 Secondary Boot Loader. I see that there is an already project, but it is based on Keil, for which i don't have a license. Can someone let me know whether it is available and if so, point me to the same ?

Regards, Biju

0 项奖励
回复
1 解答
3,206 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

An apology in advance, indeed those examples are based on Keil.

However, it is the only thing referring to the Secondary Bootloader with the LPC804.

Please excuse the inconvenience.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,213 次查看
biju_nair
Contributor III

Hi,

Unfortunately, all of these are based on Keil projects. None of them are based on MCUXpresso. Keil needs a valid license to compile.

Regards, Biju

0 项奖励
回复
3,207 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

An apology in advance, indeed those examples are based on Keil.

However, it is the only thing referring to the Secondary Bootloader with the LPC804.

Please excuse the inconvenience.

0 项奖励
回复
3,179 次查看
biju_nair
Contributor III

Thanks.

Regards, Biju

0 项奖励
回复
3,221 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

In the Documentation section of LPC80X you can find these two options, which come with their respective associated file.

nxf86756_0-1677538594891.png

Hope it helps you.

Have a nice day!

0 项奖励
回复