LPC804 - MCUXpresso based Secondary Boot Loader (SBL)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC804 - MCUXpresso based Secondary Boot Loader (SBL)

Jump to solution
3,256 Views
biju_nair
Contributor III

Hi,

I am looking at an MCUXpresso based project for LPC804 Secondary Boot Loader. I see that there is an already project, but it is based on Keil, for which i don't have a license. Can someone let me know whether it is available and if so, point me to the same ?

Regards, Biju

0 Kudos
Reply
1 Solution
3,231 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

An apology in advance, indeed those examples are based on Keil.

However, it is the only thing referring to the Secondary Bootloader with the LPC804.

Please excuse the inconvenience.

View solution in original post

0 Kudos
Reply
4 Replies
3,238 Views
biju_nair
Contributor III

Hi,

Unfortunately, all of these are based on Keil projects. None of them are based on MCUXpresso. Keil needs a valid license to compile.

Regards, Biju

0 Kudos
Reply
3,232 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

An apology in advance, indeed those examples are based on Keil.

However, it is the only thing referring to the Secondary Bootloader with the LPC804.

Please excuse the inconvenience.

0 Kudos
Reply
3,204 Views
biju_nair
Contributor III

Thanks.

Regards, Biju

0 Kudos
Reply
3,246 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

In the Documentation section of LPC80X you can find these two options, which come with their respective associated file.

nxf86756_0-1677538594891.png

Hope it helps you.

Have a nice day!

0 Kudos
Reply