LPC804 - MCUXpresso based Secondary Boot Loader (SBL)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC804 - MCUXpresso based Secondary Boot Loader (SBL)

ソリューションへジャンプ
3,084件の閲覧回数
biju_nair
Contributor III

Hi,

I am looking at an MCUXpresso based project for LPC804 Secondary Boot Loader. I see that there is an already project, but it is based on Keil, for which i don't have a license. Can someone let me know whether it is available and if so, point me to the same ?

Regards, Biju

0 件の賞賛
返信
1 解決策
3,059件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

An apology in advance, indeed those examples are based on Keil.

However, it is the only thing referring to the Secondary Bootloader with the LPC804.

Please excuse the inconvenience.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,066件の閲覧回数
biju_nair
Contributor III

Hi,

Unfortunately, all of these are based on Keil projects. None of them are based on MCUXpresso. Keil needs a valid license to compile.

Regards, Biju

0 件の賞賛
返信
3,060件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi again,

An apology in advance, indeed those examples are based on Keil.

However, it is the only thing referring to the Secondary Bootloader with the LPC804.

Please excuse the inconvenience.

0 件の賞賛
返信
3,032件の閲覧回数
biju_nair
Contributor III

Thanks.

Regards, Biju

0 件の賞賛
返信
3,074件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

In the Documentation section of LPC80X you can find these two options, which come with their respective associated file.

nxf86756_0-1677538594891.pngnxf86756_0-1677538594891.png

Hope it helps you.

Have a nice day!

0 件の賞賛
返信