LPC800 ISP connect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC800 ISP connect

1,324 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by idol on Fri Mar 01 02:30:31 MST 2013
when  we connect the isp  of lpcxpresso LPC812, We must pay attention to R55 that is connected to AD.
We must put the resistance welding down,or we cannot connect the isp
标签 (1)
0 项奖励
回复
1 回复

1,273 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheShed on Fri Mar 01 04:45:08 MST 2013
Not a great piece of design is it....

With the trimming pot wound all the way up the external uart can never pull ISP-RX below half rail. In my setup it doesn't get much below 1.9V which is well outside the limit for a valid LOW of 0.3VDD.
On the plus side, it is a 22k pot so set it to anywhere *except* against the end stop and it should be fine.

I think this highlights the one flaw I have found so far with the LPC8xx design: The two analogue compare inputs are both assigned to ISP pins. One would have been OK but not both.

Could I request that this is changed for the next part in the family - please...

--
mike
0 项奖励
回复