LPC800 ISP connect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC800 ISP connect

1,408件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by idol on Fri Mar 01 02:30:31 MST 2013
when  we connect the isp  of lpcxpresso LPC812, We must pay attention to R55 that is connected to AD.
We must put the resistance welding down,or we cannot connect the isp
ラベル(1)
0 件の賞賛
返信
1 返信

1,357件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheShed on Fri Mar 01 04:45:08 MST 2013
Not a great piece of design is it....

With the trimming pot wound all the way up the external uart can never pull ISP-RX below half rail. In my setup it doesn't get much below 1.9V which is well outside the limit for a valid LOW of 0.3VDD.
On the plus side, it is a 22k pot so set it to anywhere *except* against the end stop and it should be fine.

I think this highlights the one flaw I have found so far with the LPC8xx design: The two analogue compare inputs are both assigned to ISP pins. One would have been OK but not both.

Could I request that this is changed for the next part in the family - please...

--
mike
0 件の賞賛
返信