LPC55xx: IOCON setting, OD with on-chip pull-up resistor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55xx: IOCON setting, OD with on-chip pull-up resistor

跳至解决方案
883 次查看
AmberLin
Contributor II

Hi community,

Is it legal to config type D pin as open drain with pull-up mode?

Is there any adverse impact?

AmberLin_0-1699324385441.png

Best Regards.

Amber Lin.

标签 (1)
0 项奖励
回复
1 解答
875 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the on-chip pull-up resistor is very large,the typical value is about 50K ohm, so the driving capability is small.

So external pull-up resistor with several K ohm for the open-drain pins is recommended.

Hope it can help you

BR

XiangJun Rong

 

在原帖中查看解决方案

1 回复
876 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the on-chip pull-up resistor is very large,the typical value is about 50K ohm, so the driving capability is small.

So external pull-up resistor with several K ohm for the open-drain pins is recommended.

Hope it can help you

BR

XiangJun Rong