LPC55xx: IOCON setting, OD with on-chip pull-up resistor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55xx: IOCON setting, OD with on-chip pull-up resistor

Jump to solution
1,613 Views
AmberLin
Contributor II

Hi community,

Is it legal to config type D pin as open drain with pull-up mode?

Is there any adverse impact?

AmberLin_0-1699324385441.png

Best Regards.

Amber Lin.

Labels (1)
0 Kudos
Reply
1 Solution
1,605 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the on-chip pull-up resistor is very large,the typical value is about 50K ohm, so the driving capability is small.

So external pull-up resistor with several K ohm for the open-drain pins is recommended.

Hope it can help you

BR

XiangJun Rong

 

View solution in original post

1 Reply
1,606 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the on-chip pull-up resistor is very large,the typical value is about 50K ohm, so the driving capability is small.

So external pull-up resistor with several K ohm for the open-drain pins is recommended.

Hope it can help you

BR

XiangJun Rong