LPC55xx: IOCON setting, OD with on-chip pull-up resistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55xx: IOCON setting, OD with on-chip pull-up resistor

ソリューションへジャンプ
1,612件の閲覧回数
AmberLin
Contributor II

Hi community,

Is it legal to config type D pin as open drain with pull-up mode?

Is there any adverse impact?

AmberLin_0-1699324385441.png

Best Regards.

Amber Lin.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,604件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the on-chip pull-up resistor is very large,the typical value is about 50K ohm, so the driving capability is small.

So external pull-up resistor with several K ohm for the open-drain pins is recommended.

Hope it can help you

BR

XiangJun Rong

 

元の投稿で解決策を見る

1 返信
1,605件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the on-chip pull-up resistor is very large,the typical value is about 50K ohm, so the driving capability is small.

So external pull-up resistor with several K ohm for the open-drain pins is recommended.

Hope it can help you

BR

XiangJun Rong