LPC55S6x VREFP and VDDA connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S6x VREFP and VDDA connection

1,429 Views
RBhagat
Contributor I

Hello,

We are using LPC55S6x for our design. We are using analog input signals which are dropped down to 2.5V max. We have connected VREFP to 2.5V and we wanted to understand voltage level allowable for VDDA pin.V

As per datasheet, it is mentioned VDDA range from 1.8V to 3.6V and VREFP range from 0.985V to VDDA

RBhagat_0-1643704821297.png

 

However as per AN13033, VDDA is range of 3.0V to 3.6V and VREFP is same as datasheet. Refer snapshot

RBhagat_1-1643704898297.png

 

We have following queries, can we connect VREFP and VDDA to same voltage level as 2.5V or do we have to connect VDDA to 3.3V and VREFP to 2.5V (as per required)

Kindly do revert on same at the earliest.

Thanks,

RB

Labels (1)
0 Kudos
Reply
1 Reply

1,406 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi RBhagat 

Please refer our latest datasheet which is correct

https://www.nxp.com.cn/docs/en/nxp/data-sheets/LPC55S6x_DS.pdf

VDDA Analog supply voltage for ADC is 1.8 - 3.6 V

Vrefp ADC positive reference voltage is 0.985 - VDDA V

 

Hope this helps,

Jun Zhang

0 Kudos
Reply