LPC55S69 : elftosb-gui location ? MCUXpresso secure provisioning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 : elftosb-gui location ? MCUXpresso secure provisioning

Jump to solution
3,979 Views
trescurieux
Contributor III

Hi

I'm trying the secure boot mode of the LPC55S69

Generating the signed binary is ok, but i'm having touble with the CMFA/CMPA generation

It seems that the simplest is to use elftosb-gui to do that

I've looked everywhere on both linux and windows but could not locate it. I've found elftosb, but not the gui version.

Is it a separate download ? any hint would be appreciated.

 

BTW, I also checked the MCU Xpresso Secure provisionning tool, which can generate /flash the signed firmware but does not seem to be able to deal with the initial provisioning (CMFA/CMPA part)

Thank you in advance

Tres

Labels (1)
0 Kudos
Reply
1 Solution
3,945 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. You can download it from this link: https://www.nxp.com/search?keyword=elftosb_gui

 

Best Regards,

Ricardo

View solution in original post

2 Replies
3,942 Views
trescurieux
Contributor III

Thanks a lot !

 

0 Kudos
Reply
3,946 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. You can download it from this link: https://www.nxp.com/search?keyword=elftosb_gui

 

Best Regards,

Ricardo