LPC55S69 : FRO_32kHz accuracy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 : FRO_32kHz accuracy

Jump to solution
2,172 Views
EugeneHiihtaja
Senior Contributor I

Hi !

On page 4 of product datasheet is written :

"

32 kHz Internal Free Running Oscillator FRO. The FRO is trimmed to +/- 65%
accuracy over the entire voltage and temperature range.

"

But later on 2% and also some range is given.

What is real FRO_32kHz accuracy ?

Regards,

Eugene

Labels (1)
0 Kudos
Reply
1 Solution
2,097 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Eugene Hiihtaja

This is a typo issue. The correct FRO_32kHz accuracy should be +/- 2%. 

We will fix it in next datasheet release.

Thanks for bringing the problem to our attention.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
2,097 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Eugene

I have checked the datasheet, I can see the conflict also.

We are check it with design. I will keep you informed.

Have a nice day,

Jun Zhang

0 Kudos
Reply
2,098 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Eugene Hiihtaja

This is a typo issue. The correct FRO_32kHz accuracy should be +/- 2%. 

We will fix it in next datasheet release.

Thanks for bringing the problem to our attention.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,097 Views
EugeneHiihtaja
Senior Contributor I

Hi Jun Zhang !

i think this is good answer . Looks like is not a problem to have full crystall-less clocking of this MCU.

Regards,Eugene

0 Kudos
Reply