LPC55S69 : FRO_32kHz accuracy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69 : FRO_32kHz accuracy

ソリューションへジャンプ
2,135件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi !

On page 4 of product datasheet is written :

"

32 kHz Internal Free Running Oscillator FRO. The FRO is trimmed to +/- 65%
accuracy over the entire voltage and temperature range.

"

But later on 2% and also some range is given.

What is real FRO_32kHz accuracy ?

Regards,

Eugene

ラベル(1)
0 件の賞賛
返信
1 解決策
2,060件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Eugene Hiihtaja

This is a typo issue. The correct FRO_32kHz accuracy should be +/- 2%. 

We will fix it in next datasheet release.

Thanks for bringing the problem to our attention.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,060件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Eugene

I have checked the datasheet, I can see the conflict also.

We are check it with design. I will keep you informed.

Have a nice day,

Jun Zhang

0 件の賞賛
返信
2,061件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Eugene Hiihtaja

This is a typo issue. The correct FRO_32kHz accuracy should be +/- 2%. 

We will fix it in next datasheet release.

Thanks for bringing the problem to our attention.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,060件の閲覧回数
EugeneHiihtaja
Senior Contributor I

Hi Jun Zhang !

i think this is good answer . Looks like is not a problem to have full crystall-less clocking of this MCU.

Regards,Eugene

0 件の賞賛
返信