LPC55S69-EVK Ethernet interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69-EVK Ethernet interface

1,103 次查看
manuelheras
Contributor I

Hi,

Could some one tell me what extension board use to add Ethernet functionality to a LPC55S69-EVK board and where to get the suitable IP stack?

Thanks in advance,
Manuel

标签 (2)
0 项奖励
回复
1 回复

973 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello Manuel,

The LPC55S69 does not have an ethernet module, therefore an expansion board will not work as an onboard PHY is required. If you must use ethernet with this board, I suggest considering working on a converter using a serial interface to ethernet, however there are no ready made examples for this type of bridging.

If you can provide the requirements for your application I can recommend a different microcontroller that will fit your needs.

Best Regards,

Sabina

0 项奖励
回复