LPC55S69-EVK Ethernet interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69-EVK Ethernet interface

1,602 Views
manuelheras
Contributor I

Hi,

Could some one tell me what extension board use to add Ethernet functionality to a LPC55S69-EVK board and where to get the suitable IP stack?

Thanks in advance,
Manuel

Labels (2)
0 Kudos
Reply
1 Reply

1,472 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Manuel,

The LPC55S69 does not have an ethernet module, therefore an expansion board will not work as an onboard PHY is required. If you must use ethernet with this board, I suggest considering working on a converter using a serial interface to ethernet, however there are no ready made examples for this type of bridging.

If you can provide the requirements for your application I can recommend a different microcontroller that will fit your needs.

Best Regards,

Sabina

0 Kudos
Reply