LPC55S16.h CAN0_BASE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,235件の閲覧回数
RRD101
Contributor III

Hi there,

 

i have a question. I installed the mcan interrupt transfer example from the SDK_2.x_LPC55S16 to try my first steps with this microcontroller and CAN.

Now i had a closer look on manual and sourcecode. I found the definition of the CAN0_BASE address in the file LPC55S16.h. But the address of secure and nonsecure are is different as shown in page 14 of 1154 of the Usermanual. Now the question, whats wrong? Or have i misunderstood something, in terms of use?

0 件の賞賛
返信
1 解決策
3,208件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
There seems to be an error in the table of the user manual. The base address of the Debug Mailbox and the CAN are switched.
The NS base address of the CAN is 0x4009_D000.

I will report this issue to have it corrected in further versions.
If you have more questions do not hesitate to ask me.
Best regards,
Omar

元の投稿で解決策を見る

2 返答(返信)
3,209件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
There seems to be an error in the table of the user manual. The base address of the Debug Mailbox and the CAN are switched.
The NS base address of the CAN is 0x4009_D000.

I will report this issue to have it corrected in further versions.
If you have more questions do not hesitate to ask me.
Best regards,
Omar

3,195件の閲覧回数
RRD101
Contributor III

@Omar_Anguiano :Thank you very much

0 件の賞賛
返信