LPC55S16 - RAM backup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S16 - RAM backup

2,763 次查看
istvanmate
Contributor II

Is there a way to keep the RAM or some portion of it alive with a backup battery on the LPC55xx micro?

 

标签 (1)
0 项奖励
回复
3 回复数

2,752 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Power Domain “Always On” includes PMC(Power management controller) and RTC.

This domain always has power as long as sufficient voltage is available on VBAT ([1.8 V –3.6 V]), that is external battery.

See below pic. "Always On " domain is in red. While RAM is not controlled by "Always On " domain. So we can't keep RAM with VBAT only.

ZhangJennie_0-1638542741826.pngZhangJennie_0-1638542741826.png

Have a nice day,

Jun Zhang

0 项奖励
回复

2,735 次查看
istvanmate
Contributor II

Thanks for the quick reply.

It is what it is. I'll have to use external means to keep data alive between power cycles.

0 项奖励
回复

2,716 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome.

0 项奖励
回复