LPC55S16 - RAM backup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S16 - RAM backup

2,817 Views
istvanmate
Contributor II

Is there a way to keep the RAM or some portion of it alive with a backup battery on the LPC55xx micro?

 

Labels (1)
0 Kudos
Reply
3 Replies

2,806 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Power Domain “Always On” includes PMC(Power management controller) and RTC.

This domain always has power as long as sufficient voltage is available on VBAT ([1.8 V –3.6 V]), that is external battery.

See below pic. "Always On " domain is in red. While RAM is not controlled by "Always On " domain. So we can't keep RAM with VBAT only.

ZhangJennie_0-1638542741826.png

Have a nice day,

Jun Zhang

0 Kudos
Reply

2,789 Views
istvanmate
Contributor II

Thanks for the quick reply.

It is what it is. I'll have to use external means to keep data alive between power cycles.

0 Kudos
Reply

2,770 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome.

0 Kudos
Reply