LCP55S69 with 7inch touch screen? (feasible..?)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCP55S69 with 7inch touch screen? (feasible..?)

Jump to solution
2,313 Views
BabyBorisova
Contributor II

Hey

I'm planning to use the LCP55S69 for an LVGL project. I know there is an example project and i believe that drives a 2.8" screen.
I'm going to connect to an FT813 controller with 7in 800x480pixel display. As the controller is capable of driving this display and the requirements for PI communication to the controller are possible with the LCP board, this seems to me as a feasible option.
However, is there anything I'm overlooking? Will this evaluation board be capable of this project considering the FT813 is capable of driving the screen?

Sorry for the somewhat specific yet vague question but would love a pointer if anyone has experience with this board.

Kind regards,
Lexi

0 Kudos
Reply
1 Solution
2,301 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

We  have littlevgl_examples under MCUXpresso SDK for  Adafruit TFT LCD shield w/Cap Touch V2.3, SPI display. Besides, we don't have other existing demo.  User needs to refer our demo to adjust code by self.

There are different versions of Adafruit 2.8" TFT LCD shields. The shields marked v2.0 works directly with this project. For the other shields, please solder the center pin of IOREF pads to the 3.3V pad, and solder the pads 11, 12, and 13.
See the link for details:
https://community.nxp.com/t5/MCUXpresso-Community-Articles/Modifying-the-latest-Adafruit-2-8-quot-LC...


Besides, NXP has partnered with SEGGER Microcontroller to offer high performance embedded graphics libraries in binary form for free commercial use. FYI.
https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY

Thanks,

Jun Zhang

 

View solution in original post

1 Reply
2,302 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

We  have littlevgl_examples under MCUXpresso SDK for  Adafruit TFT LCD shield w/Cap Touch V2.3, SPI display. Besides, we don't have other existing demo.  User needs to refer our demo to adjust code by self.

There are different versions of Adafruit 2.8" TFT LCD shields. The shields marked v2.0 works directly with this project. For the other shields, please solder the center pin of IOREF pads to the 3.3V pad, and solder the pads 11, 12, and 13.
See the link for details:
https://community.nxp.com/t5/MCUXpresso-Community-Articles/Modifying-the-latest-Adafruit-2-8-quot-LC...


Besides, NXP has partnered with SEGGER Microcontroller to offer high performance embedded graphics libraries in binary form for free commercial use. FYI.
https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY

Thanks,

Jun Zhang