LPC55S04 gives bus fault and goes into hard-fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S04 gives bus fault and goes into hard-fault

2,089件の閲覧回数
KumarG
Contributor II

I am using LPC55S04 for one of my projects.  Firmware is finalized and is working fine on more than 20 boards.  

Same code when programmed into newly purchased controllers is leading to continuous hard-faults, some times bus-fault is shown while debugging, some times FORCED fault.

Debug window shows different function names every time after halting.

these controllers also has two pin-1 markers (previous controllers had only one). 

Lpc55s04.jpeg

 

Request to please help me to find out the root cause of the issue.

Regards

Kumar

 

 

ラベル(1)
0 件の賞賛
返信
9 返答(返信)

2,042件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls download SDK package from the website:

https://mcuxpresso.nxp.com/en

 

try the LED or uart example, check if you have issue.

BTW, pls try to use internal IRC.

BR

XiangJun Rong

0 件の賞賛
返信

2,027件の閲覧回数
KumarG
Contributor II

Hi,

I have tested with led_blinky project from SDK package, following are the observations.

1) Code working fine when using 12Mhz FRO clock BOARD_BootClockFRO12M();

2) Code going into hard_fault immediately when using BOARD_BootClockFROHF96M();

3) Code going into hard_fault immediately when using BOARD_BootClockPLL96M();

Regards

Kumar

0 件の賞賛
返信

2,018件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Okay, when your board runs up to 96MHz, the hardfault error occurs immediately, I suppose the firmware is correct because you use SDK example.

Maybe your board design has issue, especially the power supply part.

Can you share the power supply schematics of board so that we can have a review?

BR

XiangJun Rong

0 件の賞賛
返信

2,014件の閲覧回数
KumarG
Contributor II

Hi,

Please find the schematic of power supply part 

Lpc_Power.png

Regards

Kumar

タグ(1)
0 件の賞賛
返信

1,996件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked the schematics, I suppose it is okay.

Pls test the VDD_PMU pin voltage and check if it is the voltage you set in the software.

BTW, do you think that the 3.3V power supply can provide enough current?

BR

XiangJun Rong

 

0 件の賞賛
返信

1,985件の閲覧回数
KumarG
Contributor II

HI,

Voltage at VDD_PMU is 1.076V, programmed is 1.15V (DCDC_POWER_PROFILE_MEDIUM)

3.3V Power supply comes from LM1117-3.3 regulator, which can drive 800mA.

 

Regards

Kumar

0 件の賞賛
返信

1,964件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The VDD_PMU pin voltage does not reach to the expected.

maybe it is related to the inductor type for the DC/DC converter, pls refer to the community ticket.

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/why-is-the-spec-of-saturation-current-fo...

 

It gives the inductor saturation spec required.

Hope it can help you

BR

Xiangjun Rong

 

0 件の賞賛
返信

1,959件の閲覧回数
KumarG
Contributor II

Hi,

Inductor used is SRP2510A-4R7M 

Saturation current rating is 1.8A & rated rms is 1.36A

I have captured voltage before and after inductor, there is a large voltage spike on core voltage.

SDS00001.png

Regards

Kumar

0 件の賞賛
返信

1,866件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The DC/DC voltage delta is very high, I suppose that this is related to the 22uF capacitor.

Pls refer to the 22uF capacitor feature in the AN

https://www.nxp.com.cn/docs/en/application-note/AN12325.pdf

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信