LPC5536-EVK unable to connect wire for probe index 1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5536-EVK unable to connect wire for probe index 1

ソリューションへジャンプ
1,448件の閲覧回数
marco_xia
Contributor I

When I use the IDE tool to import hello world demo in LPC5536-EVK boards, the following error is displayed when I click debug: 

marco_xia_1-1691640660178.jpeg

The device manager displays the contents of the red box in the figure, but the three identifiers on the left are not displayed.and the MCU_LINK firmware runs normally.2.png

The software version is as follows:

MCUXpresso IDE v11.8.0_1165;SDK_2_10_2_LPCXpresso55S36;MCU-LINK_INSTALLER_3.108.exe

SO. How do I solve this problem?

thank you

ラベル(2)
0 件の賞賛
返信
1 解決策
1,368件の閲覧回数
marco_xia
Contributor I

thanks for your answer. the rootcause  maybe Trustzoom demo leads DAP err,so blhost can't connect to

EVK in ISP mode.we use keil  tools to recover it in ISP mode at last.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,416件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @marco_xia 

1) Enter ISP mode, use blhost erase all flash, also can use GUI Flash tool in MCUXpresso IDE to erase.

2)Update debug firmware.

3) Open a new IDE Workspace, import hello world demo, then debug again.

 

BR

Alice

0 件の賞賛
返信
1,369件の閲覧回数
marco_xia
Contributor I

thanks for your answer. the rootcause  maybe Trustzoom demo leads DAP err,so blhost can't connect to

EVK in ISP mode.we use keil  tools to recover it in ISP mode at last.

0 件の賞賛
返信