LPC5536-EVK unable to connect wire for probe index 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5536-EVK unable to connect wire for probe index 1

Jump to solution
1,548 Views
marco_xia
Contributor I

When I use the IDE tool to import hello world demo in LPC5536-EVK boards, the following error is displayed when I click debug: 

marco_xia_1-1691640660178.jpeg

The device manager displays the contents of the red box in the figure, but the three identifiers on the left are not displayed.and the MCU_LINK firmware runs normally.2.png

The software version is as follows:

MCUXpresso IDE v11.8.0_1165;SDK_2_10_2_LPCXpresso55S36;MCU-LINK_INSTALLER_3.108.exe

SO. How do I solve this problem?

thank you

Labels (2)
0 Kudos
Reply
1 Solution
1,468 Views
marco_xia
Contributor I

thanks for your answer. the rootcause  maybe Trustzoom demo leads DAP err,so blhost can't connect to

EVK in ISP mode.we use keil  tools to recover it in ISP mode at last.

View solution in original post

0 Kudos
Reply
2 Replies
1,516 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @marco_xia 

1) Enter ISP mode, use blhost erase all flash, also can use GUI Flash tool in MCUXpresso IDE to erase.

2)Update debug firmware.

3) Open a new IDE Workspace, import hello world demo, then debug again.

 

BR

Alice

0 Kudos
Reply
1,469 Views
marco_xia
Contributor I

thanks for your answer. the rootcause  maybe Trustzoom demo leads DAP err,so blhost can't connect to

EVK in ISP mode.we use keil  tools to recover it in ISP mode at last.

0 Kudos
Reply