LPC55 SB2.1 recovery Image loading from SPI - Is a physical reset required?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55 SB2.1 recovery Image loading from SPI - Is a physical reset required?

跳至解决方案
1,206 次查看
awseiger
Contributor I

I am reading documentation on the LPC55 SB2.1 recovery image load from SPI Flash - My company wishes to use this system for field updates. 

Once the SPI Flash recovery from an SB2.1 image is complete, does the MCU automatically run the new image, or is a physical reset required?

0 项奖励
回复
1 解答
1,188 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Reset is not needed.

But you need make sure SB2.1 file is stored  in SPI Flash and secure boot is enabled if using SPI flash recovery feature.

 

Have a nice day,

Jun Zhang

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,189 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Reset is not needed.

But you need make sure SB2.1 file is stored  in SPI Flash and secure boot is enabled if using SPI flash recovery feature.

 

Have a nice day,

Jun Zhang

0 项奖励
回复