LPC55 SB2.1 recovery Image loading from SPI - Is a physical reset required?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55 SB2.1 recovery Image loading from SPI - Is a physical reset required?

Jump to solution
1,574 Views
awseiger
Contributor I

I am reading documentation on the LPC55 SB2.1 recovery image load from SPI Flash - My company wishes to use this system for field updates. 

Once the SPI Flash recovery from an SB2.1 image is complete, does the MCU automatically run the new image, or is a physical reset required?

0 Kudos
Reply
1 Solution
1,556 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Reset is not needed.

But you need make sure SB2.1 file is stored  in SPI Flash and secure boot is enabled if using SPI flash recovery feature.

 

Have a nice day,

Jun Zhang

View solution in original post

0 Kudos
Reply
1 Reply
1,557 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Reset is not needed.

But you need make sure SB2.1 file is stored  in SPI Flash and secure boot is enabled if using SPI flash recovery feature.

 

Have a nice day,

Jun Zhang

0 Kudos
Reply