I want to use P2_0 as the capture input 0 for CTIMER1, so, starting from lpcxpresso54628_hello_world SDK example for LPCXpresso EVB, I added the following code:
#define CTIMER CTIMER1
#define TIMER_RESOLUTION_ns 100
#if 0
#define PIN_CAPTURE 2, 0
#define CAPNUM 0
#define IOCON_PIO_FUNC4 4
#elif 1
#define PIN_CAPTURE 2, 17
#define CAPNUM 1
#define IOCON_PIO_FUNC4 4
#endif
CLOCK_AttachClk(kMAIN_CLK_to_ASYNC_APB);
IOCON_PinMuxSet(IOCON, PIN_CAPTURE,
IOCON_PIO_FUNC4 |
IOCON_PIO_MODE_INACT | /* No addition pin function */
IOCON_PIO_INV_DI | /* Input function is not inverted */
IOCON_PIO_DIGITAL_EN | /* Enables digital function */
IOCON_PIO_INPFILT_OFF | /* Input filter disabled */
IOCON_PIO_OPENDRAIN_DI); /* Open drain is disabled */
ctimer_config_t ctmr_cfg;
ctmr_cfg.mode = kCTIMER_TimerMode;
ctmr_cfg.prescale = (CLOCK_GetAsyncApbClkFreq() / 1000000) * TIMER_RESOLUTION_ns / 1000 - 1;
CTIMER_Init(CTIMER, &ctmr_cfg);
CTIMER_SetupCapture(CTIMER,
kCTIMER_Capture_0 + CAPNUM,
kCTIMER_Capture_BothEdge,
true); /* Enable interrupt */
NVIC_EnableIRQ(CTIMER1_IRQn);
CTIMER_StartTimer(CTIMER);
void
CTIMER1_IRQHandler(void)
{
CTIMER_ClearStatusFlags(CTIMER,
CTIMER_IR_CR0INT_MASK << CAPNUM);
}
P2_0 is on pin 8 of J12 Analog In connector on EVB. When I connect alternatively this pin to GND and VCC, no interrupt is fired.
When I try to use P2_17 as CT1_CAP1 (pin 20 of J13 Digital connector) it works, the interrupt is triggered.
What's wrong with P2_0? It's a type A pin, but it seems it can be used as CT1_CAP0.