Conversion frecuency in ADC burst mode (LPC802)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Conversion frecuency in ADC burst mode (LPC802)

Jump to solution
1,862 Views
asier
Contributor III

Hi,

Is it possible to do conversions slower in ADC burst mode ? 

I'm doing 1 channel conversion in SEQA burst mode. Interrupt with entire sequence is enabled. 

My issue is that the interrupt callback is happening every 12us, so as soon as code leaves interrupt callback it is called again and code in main is almost blocked.

Is there any way to slow down the conversión rate ? 

Thanks in advance,

Asier.

0 Kudos
Reply
1 Solution
1,844 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi asier 

The ADC controller uses the system clock as a bus clock. We can only reduce ADC conversion time by reducing ADC working clock. No option to slow down burst conversion rate only.

ZhangJennie_0-1647416784836.png

Have a nice day

Jun Zhang

 

View solution in original post

0 Kudos
Reply
1 Reply
1,845 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi asier 

The ADC controller uses the system clock as a bus clock. We can only reduce ADC conversion time by reducing ADC working clock. No option to slow down burst conversion rate only.

ZhangJennie_0-1647416784836.png

Have a nice day

Jun Zhang

 

0 Kudos
Reply